What branch connector is required to replace a Q1B circuit breaker with a QOB circuit breaker in an NQOB panelboard?
Issue:
What branch connector is required to replace a Q1B circuit breaker with a QOB circuit breaker in an NQOB panelboard?
Product Line:
Panelboards
Resolution:
SK5668 is the bus finger or panelboard connector kit for use when replacing a Q1B branch in an NQOB panel. The kit will accept QOB breakers. This is a 3 pole kit with A, B, and C phase connectors. In a 225 amp NQOB interior, this kit will allow you to mount 6 poles of breakers whether they are 1 pole, 2 pole, or 3 pole breakers. In a 400/600 amp NQOB interior, this kit will allow you to mount 3 poles of breakers whether they are 1 pole, 2 pole, or 3 pole breakers.
Released for: Schneider Electric Canada