Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
NEMA size 4 Class 8502, 8536, or 8736 Type SF replacement lugs
Issue:
Need replacement lugs for the line or load side of a NEMA size 4 Class 8502, 8536, or 8736 Type SF contactor or starter.

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environments:
Class 8502, 8536 or 8736

Causes:
Fault conditions

Resolution:
The replacement line and/or load side lugs for the NEMA size 4 contactor or starter is part number 25050-34404.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings