How can we help you today?

Are bolt on I-line breakers still available?

Issue:
Are bolt on I-line breakers still available?

Product Line:
This applies to Frame sizes F, K, L, FY, Q4, QB, QD, QG, QJ, M, P

Resolution:
Only the LA/H, FY, QB, QD, QG, and Q4 are still available with bolt on connections. All of the others are obsolete and no longer available. Plug in breakers will fit into the same spots as the equivalent bolt on breaker without any necessary changes.

The bolt on option cannot be field installed. For the factory installed option, the 3rd character in the part number must be B for the LA/H, FY, and Q4 breakers or E for the QB, QD, and QG breakers.

It has a clamp on the I-Line jaws which enables it to meet specs calling for bolted connections.
There is a 20% adder to the price of the breaker for this option. Bolt on I-Line breakers will fit into regular I-line interiors with no modifications needed.

Picture of the connector for both bolt on and plug on

Schneider Electric Canada
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
Start your sales inquiry online and en expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings