Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a Pressure Relief Valve be ordered separately for the pumptrol Pressure Switches?
Issue:
Can a Form X Pressure Relief Valve be Field Added or Replaced for the 9013G or 9013F Pressure Switches?

Product Line:
Commercial Pressure Switches

Environment:
NEMA Class 9013 Pressure Switches

Resolution:
Form X pressure release valve is  factory modification only and cannot be added in the field. The valve can be replaced on switches that were delivered with Form X. However, this is not a field retrofit for products that were not delivered with the Form X. For replacement use 9049A56 for 9013FSG and 9049A12 for 9013GHG and 9013GSG.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings