Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are field installable isolated alarm contacts available for the Class 9065 Motor Logic Overload Relays?
Issue:
Field installable Aux contact for 9065 Solid State Overload

Product Line:
NEMA and Definite Purpose Contactor and Starter

Environment:
9065 Motor Logic overload relay

Resolution:
Yes order Class 9999 Type AC04, normally open or normally closed dependent upon installation position.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings