Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a longer adjustable length lever arm than a 9007HA1 for a 9007 type C limit switch ?
Issue:
Adjustable Lever Arms for 9007 Type C Limit Switches

Product Line:
Limit Switches

Environment:
9007 Type C switch

Resolution:
Use a 9007S9 hub, 9007R16 or R17 clamp for rod or keystock, and 9007R18 or R19 or R20 roller per Digest 172 pp. 19-7 and 19-17 . 1/4`` keystock or 3/16`` rod needed may be cut to the desired length. The rod or keystock is not supplied by Sq D.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings