Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for a QMB3606T ?
Issue:
Replacement switch unit

Product Line:
Panelboards

Environment:
QMB

Cause:
Cross Ref

Resolution:
If the switch is installed on a QM interior (31`` wide box) built before 1961 there is no replacement available. If the switch is installed on a QM interior (31`` wide box) built after 1961 but before 1984 the replacement is a QMB362T. If the switch is installed on a QW interior (38`` wide box) built before 1984, the replacement would be a QMB362T along with a QMB306EX.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings