Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement handle part number for the 2601 drum switches?
Issue:
What are the replacement handle part numbers for all of the 2601 class drum switches?

Product Line:
2601 reversing drum switches

Environment:
Products sold and used in the United States

Cause:
Need a replacement handle for the 2610 reversing drum switch

Resolution:
See table below:
DescriptionPart numberStatusQuantity Required
AG2AH2BG1AW2BW1AF2BF1
Handle (standard one piece)2917A5X1AVAILABLE11-1-1-
Handle (standard one piece)2917A5X2AVAILABLE--1-1-1
Ball & Shaft Handle (optional) 2917C19G1OBSOLETE11-1-1-
Ball & Shaft Handle (optional) 4087C11G1OBSOLETE--1-1-1
Fluted Handle (optional)4087A2X1OBSOLETE11-1-1-
Fluted Handle (optional) 4087A2X2OBSOLETE--1-1-1
Handle Screw 8-32 x 3/8"2191614121AVAILABLE1111111

All special handle options have been obsolete, only the standard device is available at this time.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings