How can we help you today?

Can a 9001 KR9 be illuminated to make a 9001 KR9P?

Issue:
Trying to convert the 9001SKR9 to 9001SKR9P

Product Line:
Push Buttons and Operator Interface

Environment:
9001K/SK Heavy duty Operators

Resolution:
Yes. The only difference between the illuminated and non-illuminated devices is the square translucent spacer or liner on the back of the non-illuminated device. Remove the liner and add the light module. Also if the 9001 KR9 has a black or orange knob these will have to be changed because they are opaque.