Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum panel thickness for the 22 mm pushbuttons?
Issue:
Identify the panel thickness for the 22 mm pushbuttons

Product Line:
Harmony 22 mm Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:
6 mm is maximum panel thickness. This is true for all the 22mm push button lines.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings