Can we change a 9001 KS43B to a 9001 KS42B?
Issue:
configuration of 9001KS43B to change into 9001 KS42B
Product Line:
30mm Push Buttons
Environment:
Harmony 30 mm 9001 K Metal Push Buttons
Resolution:
Yes, order a 9001 K13B cam and change the cam. The cam snaps into place. Use screw driver or needle nose pliers to remove cam, being careful to install replacement cam in the same orientation.
configuration of 9001KS43B to change into 9001 KS42B
Product Line:
30mm Push Buttons
Environment:
Harmony 30 mm 9001 K Metal Push Buttons
Resolution:
Yes, order a 9001 K13B cam and change the cam. The cam snaps into place. Use screw driver or needle nose pliers to remove cam, being careful to install replacement cam in the same orientation.
Released for: Schneider Electric Canada