How can we help you today?

What is the part number for the contact mounting block in a 9002AW124 foot switch?

Issue:
Part number for the contact mounting block in a 9002AW124 foot switch

Product Line:
Push Buttons and Operator Interface

Environment:
Heavy Duty 9002 Industrial Foot Switches


Resolution:
Part number is 2502-D21-G1.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: