How can we help you today?

What is included in an HOMVP1 load center value pack?

Product Line:
Load Center

Resolution:
The HOMVP1 is now obsolete and no longer available. When available, it included an HOM3040M200TC load center (with combination cover and equipment ground bar), (5) HOM120 breakers, and an HOM230 breaker.

The replacement for the HOMVP1 is HOM3060M200PCVP, which includes an HOM3060M200PC load center (with combination cover), (3) HOM120 breakers, and (2) HOM230 breakers.

Schneider Electric Canada
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
  • Product Selectors