Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What size hex wrench is needed for the wire binding screw of the AL400LA lug for the LA, LH, and Q4 circuit breakers?
Issue:
What size allen wrench do you need for the  wire binding screw for the AL400LA lug?

Product Line:
Molded case circuit breakers

Resolution:
A 3/8" Allen wrench for the wire binding screw and Torx T40 is the tool used to remove or install the mounting screw.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings