Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement coil cover for 8502SE contactor?
Issue:
Identify a replacement coil for a NEMA contactor

Product Line:
Class 8502 NEMA Contactors

Environment:
Square D NEMA Contactors and Starters

Resolution:
For 2 & 3 pole devices only 31074-054-01, secured by (2) 21916-16281 mounting screws.(This applies to devices with date codes of 9202 or newer) Cover does not include nameplate nor is nameplate available. This also applies to all 8536SE, 8538SE, 8539SE, 8606SE, 8630SE, 8640SE, 8702SE, 8736SE, 8738SE, 8739SE, and 8810SE devices.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings