Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum temperature of the water (the medium) that can be used in a 9013 type F pressure switch?
Product line:
9013 pressure switches

Resolution:
125 degrees Celsius or 257 degrees F

Schneider Electric Canada

Attachment(s)
9013 Troubleshooting 9013DB0701.pdf [100.93 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings