Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU464, series F5? (may be shown as F05)
Product Line:
Heavy Duty Safety Switches, catalog number HU464, Series F5

Resolution:
The repair parts for the HU464, series F5 (F05) are as follows. These are the parts that can be replaced. No other parts are replaceable.
Complete Line/Load Base (all one piece) - 4056704150 - (requires one line base per switch - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line/Load Base mounting screws - 40205-464-01 (requires 12 per line base)
Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - 40251-162-51 (per lug)
Lug Assembly mounting screw - 21401-222-40
Switch Mechanism - 40567-401-50
Switch Mechanism mounting screws- 22999-405-62 (requires 2)
Handle Assembly - 40567-468-50
Lockplate - 40567-467-01
Lockplate mounting screws - 22999-405-62 (requires 2)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings