Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does SquareD/Schneider Electric offer Mini Power Zones (MPZ) in NEMA 12 enclosures?
Issue:
NEMA 12 Enclosures

Product Line:
LV Transformers

Environment:
Applies to Mini Power Zone (MPZ) Transformers by SquareD/Schneider Electric

Cause:
Transformers may require an enclosure rating of NEMA 12

Resolution:
SquareD/Schneider Electric currently does not offer UL listed NEMA 12 rated low voltage MPZ  Mini Power Zone dry type transformers, Ventilated or Non-Ventilated Transformers.  An exception is certain 9070 Class Transformer Disconnects. If oil tight is not a specific requirement, our Non-Ventilated and Epoxy Resin Encapsulated Transformer products may represent a suitable product for wet or dusty environments. Contact your local distributor or SquareD/Schneider Electric sales office with your environmental requirements.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings