Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the 2510 MBR1 available in an aluminum enclosure?
Issue:
Identify if there is an aluminum option for an enclosed manual starter

Product Line:
Class 2510 Manual Starters

Environment:
NEMA Contactors and Starters

Resolution:
These NEMA 7 & 9 enclosures are cast iron. NEMA types 4 X, 7 & 9 cast aluminum are available for outdoor use; to order this type of enclosures , replace the "R" in the catalog number with a "T". Example: 2510 MBR becomes 2510 MBT. This also applies to 2510 MBR2, 2510 MCR1, 2510 MCR2, 2510 MCR3, and 2510MCR5 devices.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings