Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DT223, series F5? (may be shown as F05)
Issue:
Repair parts

Product Line:
Double Throw Safety Switch

Resolution:

The repair parts for the DT223, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056775350 (one each upper and lower; arc suppressor and wire assembly not included)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Load Base - 4056683250 (one each upper and lower; lugs and wire assembly not included)
-Load Base mounting screws - 4020515101 (2 required per load base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screws - 4020514501 (1 required per arc suppressor)
-Wire Assembly - 4056621050 (1 required per phase; includes cable factory connected mechanical lug at one end and at other end, a crimped connector; use lug mounting screws)
-Line and Load Lug Assembly - 4025101851 (per lug)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101851 (per lug)
-Ground Lug mounting screw - 4020514801
-Switch Mechanism - 4056646950 (each for upper and lower)
-Linkage Assembly - 4056614950 (links together upper and lower switch mechanisms)
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562 (2 required)
-Cover Latch - 4056607201 (each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (each for upper and lower; also requires cover latch)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings