Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are replacement contacts available for 8910, 8911, and 8965 contactors?
Issue:
8910, 8911, 8965 replacement contact kits

Product Line:
Contactor and Starter Replacement Part Kits

Environment:
Class 8910, 8911 and 8965 Contactors
Resolution:
For replacement contacts for 8910, 8911, and 8965 contactors, see table below. Check the amp rating of your contactor to know the replacement contact part #. Please take note that 9998DRC* replacement contact kits contain 1 pole only.

Example:  For the 2-pole 50A contactor 8910DPA52, use the 9998DRC5 replacement contact kit.  Since the 9998DRC5 contactor is 2-pole, qty. 2 of 9998DRC5 is required.


Replacement contact kits

Note: For use with Series B devices only. Series A devices do not have replaceable contacts.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings