Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H223N series F5? (may be shown as F05)
Issue:
Repair Parts for H223N series F5

Product Line:
Safety Switch

Resolution:
The replacement parts for the H223N, series F5 (F05) are as follows. No other parts are available.
  • Interior kit - HSIF210F (includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
  • Load base kit - HLB210F (includes load base and mounting hardware).
  • Arc Suppressor kit - HAS0610F (includes arc suppressor and mounting hardware)
  • Lug kit - AL10F (includes 6 lugs)
  • Handle/Mechanism kit - HM0610F (includes handle, mechanism, lockplate, and mounting hardware)
  • Neutral Assembly - SN0610 (includes neutral assembly and bonding screw)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings