How can we help you today?

What are the repair parts for the DT322, series F5? (may be shown as F05)

Issue:
Repair parts

Product Line:
Double Throw Safety Switch

Resolution:
The repair parts for the DT322, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056603950 (one each upper and lower; order arc suppressor and wire assembly separately)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Load Base - 4056604750 (one each upper and lower; order lugs and wire assembly separately)
-Load Base mounting screws - 4020515101 (2 required per load base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly - 4056609750 (1 required per phase; use lug mounting screws)
-Line and Load Lug Assembly - 4025101652 (per lug - line, load)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101652 (per lug)
-Ground Lug mounting screw - 4020513503
-Switch Mechanism - 4056646950 (each for upper and lower)
-Linkage Assembly - 4056614950 (links together upper and lower switch mechanisms)
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940592 (2 required)
-Cover Latch - 4056607201 (each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (each for upper and lower; also requires cover latch)