How can we help you today?

What are the repair parts for the DT363RB, series F5? (may be shown as F05)

Issue:
DT363RB, series F5 field replaceable parts.

Product Line:
Safety Switch

Resolution:
The repair parts for the DT363RB, series F5 (F05), are as follows. No other parts are available.
-Line Base - 40567-751-50 (one each upper and lower; order arc suppressor and wire assembly separately)
-Line Base mounting screws - 40205-151-01 (3 required per line base)
-Load Base - 40566-046-50 (one each upper and lower; order lugs and wire assembly separately)
-Load Base mounting screws - 40205-151-01 (2 required per load base)
-Arc Suppressor Assembly - 40566-355-50 (1 required per line base)
-Arc Suppressor mounting screw - 40205-145-01 (1 required per arc suppressor)
-Wire Assembly - 40566-210-50 (1 required per phase; includes cable factory connected mechanical lug at one end and at the other end a crimped connector; use lug mounting screws)
-Line and Load Lug Assembly - 40251-018-51 (per lug - line, load)
-Line, Load Lug mounting screw - 40205-142-02
-Ground Lug - 40251-018-51 (per lug)
-Ground Lug mounting screw - 40205-148-01
-Switch Mechanism - 40566-469-50 (each for upper and lower)
-Linkage Assembly - 40566-149-50 (links together upper and lower switch mechanisms; also replace linkage assembly rubber gaskets)
-Linkage Assembly Rubber Gaskets - 40503-228-01 (3 required)
-Linkage Assembly mounting screws - 22999-405-62 (7 required)
-Handle - 40566-887-50 (handle gasket also required; lockplate gasket may also need replacing)
-Handle gasket - 40566-086-01
-Lockplate - 40566-733-01 (lockplate gasket also required)
-Lockplate gasket - 40566-086-01 (1 required)
-Lockplate mounting screws - 22999-405-62 (2 required).

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: