Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is replacement control coil available for 8910DPA122V08?
Issue:
8910DPA122V08 replacement coil

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8910 DP,DPA Definite Purpose Contactors

Resolution:
31074-400-44 for 60 hertz applications only, coil consumption is 700 VA inrush, 46 VA sealed for 60 hertz applications.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings