Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is replacement coil available for 8911DPSG22V02?
Issue:
Are replacement coils available for the 8911DPSG22V02?

Product Line:
Nema Definite Purpose Contactors

Environment:
Maintenance

Cause:
Coil Replacement

Resolution:
Coil part number 9998DA1V02, coil consumption is 56 VA inrush and 6 VA sealed. However this was the coil for the Series A or B DP contactor and is now obsolete with no replacement.  The contactor itself must be replaced.  Series C coils will not fit the Series A or B contactor.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings