Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are replacement contacts available for 8965RO10?
Issue:
Are replacement contacts available for 8965RO10?

Product Line:
Class 8965 Contactors

Environment:
Hoist Contactors

Cause:
Replacement Components

Resolution:
The replacement kit depends on the device series. The following outlines the correct replacement kit: Series A or Series B - 9998RA10, Series C - 9998RA14.
This kit consists of the complete stationary contact block assembly, contact springs and 6 movable contacts. Enough for one complete reversing hoist contactor.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings