How can we help you today?

What terminations are available on the HC8SN?

Issue:
HC8SN I Line solid neutral wire size

Product Line:
Panelboards

Environment:
I-Line Power Distribution Panelboar

Resolution:
Terminations are as follows:

Main Lugs
(4) #3/0 - 750MCM

Branch
(34) #4 - 14 AWG
(9) #14 - 1/0 AWG
(7) #6 - 350MCM