How can we help you today?

What are the repair parts for an H226N, series E2 and E4 heavy duty safety switch?

Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN226NE2 (includes line & load base assembly, neutral assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 4055218550SEL (2-required and arc suppressor assembly is not included)
Load base assembly - 4055218750SEL (2-required)
Arc suppressor assembly - 4051270850SEL (2-required)
Lug assembly - 4405044601 (2 required per base assembly)
Neutral assembly - H600SN
Line base phase insulator - 4051201401 (1 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit (black & red knob at end of handle) - Series E2 is 4401142750, Series E4 is 4028343550
Neutral bonding strap - 4028300750SEL (also fits H226N series E1 switch)
Cross Arm Insulator – (2) 4055217701 (left and right side pieces); (1) 4055217801 (center piece); (1) 4055215701 (dust shield – retainer for insulators)

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings