How can we help you today?

What are the repair parts for a H228NAWK, Series E4?

Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4401139254 (2 required; arc suppressor assembly is not included)
Load base assembly - 4401139351 (2 required)
Lug assembly - 4405005402 (1 required per base assembly)
Neutral assembly - H1200SNE4
Line base phase barrier - 4401119501 (1 required)
Line base insulating plug - 4401133901
Handle assembly - 4401141351
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit - 4028343550
Neutral bonding strap - 4401134250SEL
Crossbar Insulator Kit - 4051275250 (note: the metal cross bar is not replaceable)
Fuse Mounting Hardware - Bolt = 2140128481, Nut = 2342702800, Washer = 2360100280

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: