How can we help you today?

Can an XD4 with maintained operation be field converted to spring return?

Issue:
Can an XD4 joystick with maintained operation be field converted to spring return?

Product Line:
Digest 177 Section 19 : Push Buttons and Operator Interface

Environment:
North American Products

Resolution:
No, the device cannot be field converted. An entire new joystick would need to be ordered with the desired functionality.

Schneider Electric Canada
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
  • Product Selectors