How can we help you today?

Can the operating handle of an FA060Y circuit breaker enclosure be padlocked in the OFF position?

Product Line:
Circuit Breaker Enclosures

Resolution:
Yes, the external operating handle is provided with integral provisions for padlocking the handle in the OFF position ONLY. With the external operating handle in the OFF position, push the padlock provision tab located on the handle back, which will then allow a padlock to be placed around the handle.
NOTE: WITHOUT PUSHING THE LOCKING PROVISION TAB ON THE HANDLE BACK, A PADLOCK COULD BE PLACED AROUND THE HANDLE, BUT IT WOULD NOT LOCK THE HANDLE IN PLACE. THE LOCKING PROVISION TAB MUST BE PUSHED BACK TO ACTIVATE THE LOCKING MECHANISM.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors