Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the GV2AF3 and the GV2AF4?
Issue:
Checking on the difference between the GV2AF3 and the GV2AF4.

Product Line:
GV Manual Motor Starters and Protectors

Environment:
IEC Contactors and Starters

Resolution:
The GV2AF3 allows the GV2/LS1D to be mounted to the TeSys contactor so that the back of the devices are aligned. The GV2AF4 allows the GV2/LS1D to be mounted to the TeSys contactor so that the front of the devices are aligned. If the GV2AF4 is used, the LAD31 also has to be installed in order to mount the assembly to DIN rail.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings