Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement lug for a QOM circuit breaker?
Issue:
Can I replace the lugs on a QOM breaker?

Product Line:
Circuit Breakers

Resolution:
The lugs on the QOM circuit breakers are not replaceable (they are riveted on). If a lug has been damaged, the circuit breaker will need to be replaced.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings