Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
9007 J Can I get a longer Delrin extension?
Issue:
Is it possible to get a longer Delrin for 9007 J?

Product Line:
Pressure, Vacuum, and Float Switches

Environment:
Limit Switches

Resolution:
The Delrin original is 2 7/8 (2.85)`` total length, .35`` goes into the spring, 2.5`` extends beyond the spring. Other Delrin lengths which have been manufactured are: 9007J S2 15 9/16; 9007J S4 22 9/16; 9007J S5 33 9/16; 9007J S6 10 9/16; 9007J S7 5 7/8; 9007J S9 10 1/4. Check Quote to Cash for availability as some may be obsolete.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings