Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are QO/QOB-EPD breakers rated for heat trace?
Issue:
Heat Trace compatibility of QO/QOB - EPD breakers

Product Line:
Circuit Breakers

Resolution:
Yes. The ground fault protection level is 30 milliamps, which is rated to protect electrical equipment such as heat trace tape.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings