Issue:
Oversized enclosure on 8538/39 combination starters
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
NEMA combination starters
Resolution:
For NEMA sizes 0 through 2 only. See 8538 and/or 8539 selection pages of current Digest for ``S8`` oversized enclosure option. For devices not setup, Form G28 is also a possible option.
Oversized enclosure on 8538/39 combination starters
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
NEMA combination starters
Resolution:
For NEMA sizes 0 through 2 only. See 8538 and/or 8539 selection pages of current Digest for ``S8`` oversized enclosure option. For devices not setup, Form G28 is also a possible option.
Released for: Schneider Electric Canada