Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement overload relay for an 8536SF NEMA Size 4 starter?
Issue:
8536SF NEMA Size 4 overload replacement

Product Line:
NEMA and Definite Purpose Contractors and Starters

Environment:
9065 Overloads

Resolution:
The replacement overload relay depends upon the device used and any Forms originally ordered. The following outlines the replacement parts:

Three pole starter with melting alloy (no overload form), 9065SDO15.
Four pole starter with melting alloy (no overload form), 9065SDO16.
Five pole starter with melting alloy (no overload form), 9065SDO17.

Overload relay Form H30, 9065ST420.
For Series F of the MotorLogic solid state overload relay, they are capable of protecting single phase load.
See following link as reference: https://download.schneider-electric.com/files?p_enDocType=Instruction+sheet&p_File_Name=30072-013-29_01.pdf&p_Doc_Ref=30072-013-29

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings