Do the QO2100BNS, QO2100BNF, QO2100BNRB, QO2125BNS, QO2125BNF, and QO2125BNRB circuit breaker enclosures include a solid neutral?
Issue:
Product Design Features
Product Line:
QO Circuit breaker enclosures
Resolution:
Yes, a bondable neutral is supplied as standard with these catalog numbers.
NOTE: The 'N' in the catalog number signifies the neutral assembly factory installed, e.g. QO2100BNS.
Product Design Features
Product Line:
QO Circuit breaker enclosures
Resolution:
Yes, a bondable neutral is supplied as standard with these catalog numbers.
NOTE: The 'N' in the catalog number signifies the neutral assembly factory installed, e.g. QO2100BNS.
Released for: Schneider Electric Canada