Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will an SL800 subfeed lug kit fit into an HCM I-Line panel interior?

Issue:
SL800 kit characteristics

Product Line:
Panelboards

Environment:
I-Line HCM

Cause:
Mounting

Resolution:
Yes, the SL800 subfeed lug kit will fit into an HCM I-Line panel interior .

UPDATE (2018): The SL800 is now replaced by the SL800M5 subfeed lug kit.  This is rated for (3) - 3/0 to 500 MCM conductors. This will work in the HCM, HCP, HCP-SU and HCR-U I-Line
panelboards

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings