Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a NEMA 4X fiberglass enclosure available for the NF panelboard?
Issue:
Is NF panelboard available in NEMA 4X fiber glass enclosure?

Product Line:
Square D panelboard

Environment:
NF panelboard

Resolution:
It is available as a factory assembled option for an NF panel. The maximum allowable height is 50`` and the interior is limited to 250A maximum.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings