Are any of the general duty, heavy duty, or double throw, NEMA 3R enclosure safety switches available in stainless steel enclosures?
Issue:
Product design features
Product line:
General Duty, Heavy Duty and Double Throw Safety Switches
Resolution:
No, the material of the NEMA 3R enclosure is galvanneal painted steel. However, the NEMA 4, 4X, 5 stainless steel switches (suffix DS or SS) are suitable for NEMA 3R applications by removing the drain screw from the bottom endwall of the enclosure.
Product design features
Product line:
General Duty, Heavy Duty and Double Throw Safety Switches
Resolution:
No, the material of the NEMA 3R enclosure is galvanneal painted steel. However, the NEMA 4, 4X, 5 stainless steel switches (suffix DS or SS) are suitable for NEMA 3R applications by removing the drain screw from the bottom endwall of the enclosure.
Released for: Schneider Electric Canada