Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ZB2BW060 come with a bulb?
Issue:
Identify if the ZB2BW060 come with a light

Product Line:
22 mm Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:
The ZB2BW060 comes with a bulb if you put voltage needed as a suffix at the end of the part number such as ZB2BW060120v. If you do not put the voltage code on the part number it will come without a bulb.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings