How can we help you today?

Can you put a mushroom button on a 9001KR1U or a 9001SKR1U?

Issue:
Mushroom button on a 9001K/SKR1U

Product Line:
Harmony 30 mm 9001 K/SK Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:
Yes, the snap in mushroom buttons will fit on these operators.