Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H328N, series E4 heavy duty safety switch?
Issue:
Repair parts for H328N Series E4

Product Line:
Heavy Duty Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4401139254 (3 required; arc suppressor assembly not included)
Load base assembly - 4401139351 (3 required)
Lug assembly - 4405005402 (1 required per base assembly)
Neutral assembly - H1200SNE4
Line base phase barrier - 4401119501 (2 required)
Line base insulating plug - 44011-3901
Handle assembly - 4401141351
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit - 4028343550
Neutral bonding strap - 4401134250SEL
Crossbar Insulator Kit - 4051275250 (note: the metal cross bar is not replaceable)
Fuse Mounting Hardware - Bolt = 2140128481, Nut = 2342702800, Washer = 2360100280

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings