Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement contact for an 8501XMO?
Issue:
What is the replacement normally closed contact for an 8501XMO master relay?

Product Line:
Relays and Timers

Environment:
Class 8501 Type X Relays

Resolution:
The 8501XC4 is the primary contact cartridge. It can be installed as normally open or closed. A maximum of 6 primary contacts can be installed in an AC or DC controlled relay.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings