Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Square D offer a tool/device to test a Hospital Isolated Power panel system?

Issue:
Testing Medical Products

Product Line:
LIMs and Isolation Panels

Environment:
Hospital and clinics

Cause:
Tester for setup and troubleshooting

Resolution:
While Schneider Electric/Square D offered a device for this at one time, it is no longer offered as there are now suitable OEM devices to serve this purpose that are smaller and less complicated to use, as well as less expensive,  In addition to this device, a multitester with milliamp metering capabilities is required.

One OEM to offer a Line Isolation Monitor test device is Bender Inc. and another is Dale Technologies

Bender Inc.
484-288-7500
http://bender.org/

Dale Technologies (formerly DNI Nevada)
(800) 544-DALE (3253)
http://www.daletech.com

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings