Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between a XS4P18AB110 and XS4P18AB120?
Issue:
Identifying product differences

Product Line:
Inductive Sensors

Environment:
Products Sold in North America

Resolution:
They are both inductive proximity sensors with a analog output.
(2 wire) AB110 is 4-14 mA output and the AB120 is 4-20mA output.
(3 wire) AB110 is 0-10 mA output and the AB120 is0-16mA output.

Also the AB110 is rated 24-48 volts.


Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings