Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the accuracy rating of the metering CTs for Masterpact NW breakers?
Issue:
What is the accuracy rating of the metering CTs for Masterpact NW breakers?

Product Line:
Masterpact

Resolution:
The CTs were designed for C37.20.1 metering accuracy.
All metering transformers are accurate with the 0.3% accuracy class, 5 A output ratio at full load (for example, a 1600 A metering CT would send 5 A at the full load of 1600 A).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings