Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What was the maximum ampere rating for the legacy MA frame breaker which could be installed in an I-Line panelboard?
Issue:
legacy MA Characteristics

Product Line:
I-Line Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 29 & 94-1989, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2000 IBC, 1995 NBCC

Cause:
The legacy MA (and related higher AIR frames such as MH, MX, ME) were available in higher ampere ratings; however, these higher ampere ratings were never available with an I-Line jaw for installation in an I-Line panelboard or the I-Line distribution section of a Power-Style or QED2 switchboard.

Resolution:
800A was the maximum ampere rating for an MA frame I-Line branch breaker. This required an HCWM interior. For 900A or 1000A ratings, the legacy NA frame had to be used. The ``N`` frame breaker required an HCWM-U interior (now obsolete) or an HCR-U interior. Both the MA frame and NA frame circuit breakers are now obsolete.  The MA frame is superseded by either the Powerpact M or Powerpact P circuit breaker, according to application details.  The NA frame circuit breaker is superseded by either the Powerpact P or Powerpact R circuit breaker according to application details.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings